08-13-2024 09:04 PM
I would like to automatically configure the Ethercat master without the use of the IO engineer tool. Is there a specification for the XML config file that the ethercat master references?
09-02-2024 02:43 PM - edited 09-09-2024 12:52 PM
As the EtherCat master does not work with any syntax error in the XML file we do not recommend to set them up "by hand" but use ctrlX IO Engineering. Depending on your application you could also add several description files on the control and switch between them via our solution management (active and archived configuration)