03-01-2024 02:34 PM
Hello everyone,
I want to use the Profinet Device App on the ctrlX CORE X3 Plus.
And I am wondering if it is possible with this app to communicate cyclic and also acyclic?
I just found out that the cyclic communication should work but also the acyclic?
Thanks in advance.
03-08-2024 12:23 PM
Could more define what you are expecting to read acyclically? As the ctrlx CORE would be a Profinet Device but does not have the parameters known from a drive.
09-05-2024 01:16 PM
Are there any news? can this topic be closed?