FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
02-16-2023 12:32 AM
I am wanting to interface a Beckwith M-3410A protection relay to the CtrlX core. We are already using the Modbus TCP app. Can I use a modbus gateway to convert RTU to TCP in order to communicate with the core? Is it possible to use the USB-C port on the core for this, or must I use an ethernet port (XF10 and/or XF51)?
Solved! Go to Solution.
02-17-2023 09:17 AM
There are different ways to directly connect Modbus RTU to the ctrlX CORE.