FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
12-11-2023 06:27 AM
Hello,
Are there any example / some one who has tried to communicate CtrlX with the Fanuc 0iTD CNC controller.
unfortunately fanuc controller is not supported on DeviceBridge Ctrlx App, so trying if we have any other method to communicate with Fanuc 0iTD controller.
Thanks in advance
12-11-2023 08:00 AM
Moved to corresponding sub forum "Communication".
What protocols/interfaces are supported by the FANUC controller and which data you like to exchange?
12-12-2023 10:55 AM
Hello,
the Fanuc controller interface, inside the Ctrlx DeviceBridge app, is dependent on the used hardware.
With an X3 (ARM based control), the Fanuc controller is not available. With an X7 (or upcoming X5), an x86 based control, the Fanuc controller is available. The resason for this, is a x86 based Fanuc library, that is used inside the DeviceBrigde app
Which interfaces are provided by the Fanuc 0iTD CNC controller? If the controller Fanuc offers an OPC UA server, this would be the preverd way.
Thursday
@Nithin Are there any news? Can this topic be closed?