Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Bridge Port XF51 as 'Switch'

Bridge Port XF51 as 'Switch'

tomtw1
Member

Hello,

Sometimes we have a situation where we connect several devices to a switch. A number of times we already used all the available ports and we were only one port short, resulting in an extra switch. To solve this issue I would like to know if it would be possible to configure the XF51 port so that it would be possible to have communication between the laptop and the HMI in the image below. 

3 REPLIES 3

CodeShepherd
Community Moderator
Community Moderator

In general it is not possible to use the same subnet on both ports (192.168.1.x on XF10 and XF51) as the IP stack would not to which port the communication packages should be send. 

To what should the PC should have access to? Only to the ctrlX CORE (easy to achieve) or to all participants in the XF10s network (more complex to achieve)?

Hi,

Thanks for your reply. I would like to have acces to all participants, otherwise it would not be helpfull. I can imagine that it's hard to achieve, but I was curious if it still would be possible.

CodeShepherd
Community Moderator
Community Moderator

Thanks to a hint of @TheCodeCaptain. In the current version 2.6 it is possible to add a bridge to the ports XF10 and XF51 to act as the same port. Switch of security if asked and beware that IP address changes to 192.168.2.1:

ctrlX web UI - add network bridgectrlX web UI - add network bridge

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist