FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-27-2021 08:56 AM
Do the ctrlX CORE support BACnet? If they do, how should the CORE be configured?
Thanks!
Solved! Go to Solution.
10-28-2021 08:44 PM
Hi redford,
at the moment BACnet is not supported from ctrlX CORE, it is in the backlog.
But, it is possible to have a hybrid solution with the BACnet certified XM21 controller. See how it works in youtube
If you want, we can look deeper in your requirement, please get direct in touch with me.
Thanks !
11-16-2021 11:33 AM
Some mistake in the link for Bacnet @youtube.
Please check this: Youtube
08-30-2024 08:08 PM
Hello @steff ,
Is BACnet still unsupported in ctrlX?
I see that the 'CmpBACnet' library from Codesys is available in PLC Engineering 2.6.2, however this appears to require an add-on similar to what's used in the Codesys EtherNet/IP and Profinet drivers.
09-02-2024 07:47 AM
Hallo,
in the second half of 2024 there will be also a BACnet.app available. It is realized from MBS, one of the ctrlX World partner.
Regards
Sozu