12-12-2022 11:46 AM
Hello,
The S7-1200 communicates with the CTRLX3 (XF51) profinet and cannot communicate normally. At present, it is unknown where the settings are incorrect or other situations. Does anyone know?
Solved! Go to Solution.
12-13-2022 11:08 AM - edited 12-13-2022 11:08 AM
Hello Hui,
faced similar topic some days ago and the rootcause in not finally closed and confirmed.
Could you please operate with a different PNIO Module testwise. The variety of moduels you can use is quite big - but I assume not all of them are supported right now (by the S7..).
Please configure the S7 and ctrlX-PLC with a PN-INOut64Byte and try to run the connection.
I checked several modules between ctrlX running as PNController and a 2nd ctrlX running as PN-Device and that worked unsuspiously.
Bye
Please add the PLC-Logger info with further infos regarding the test.
01-16-2023 08:23 AM
Any news here or can this topic be closed?