06-26-2024 11:03 AM - last edited on 07-02-2024 07:17 AM by CodeShepherd
Hello
Customer is using 02V06 release - he is trying to read Keyence code reader via XF51 with X3 Core with 02V06 Release. we are using codesys fieldbus profinet controller
When we scan the keyence controller - we get error as "not able to read the ID number"
Atatched GSDML file and error video with screenshot.
Same Keyence code reader working with XM21 and XFE as profinet controller
Kindly suggest
07-01-2024 09:32 AM
As the error message is suggesting that RCP telegram is blocked because of e.g. firewall settings please check this topic.
Also check CODESYS documentation for further explanation or help as this is 3rd Party product from them.
07-01-2024 01:08 PM
Hi
We added inbound rules - not much clarity in documentation too
Same module is working with XM and Siemens PLC.
Customer not able solve this issue