05-31-2022 10:10 AM
Hi all,
I have imported into the PLC environment the library from "codesys IIOT library package". And try to create a working project with the COREvirtual. To start with, I opened the example project which is inserted with this library from the MQTT Client SL.
I keep getting the following error:
Internal error:System.NullReferenceException: The object reference is not set to an instance of an object.
It seems that this error has to do with the visualization because as soon as I remove it I can download the project.
AFTER I set the viral core to version 1.8.0.
With new version I get the following error:
[FATAL ERROR] Unresolved reference: 'CODEMGETCONTENTBYFIRMCODE2'.
[FATAL ERROR] Unresolved reference: 'CODEMGETCONTENTBYFIRMCODE2'.
I would like to use the attached visualization and run tests with the MQTT client in combination with a CORE virtual.
Anyone who has managed to do this? Would love to hear about it!
Solved! Go to Solution.
06-01-2022 03:49 PM - last edited on 11-24-2022 07:42 AM by CodeShepherd
ctrlX CORE virtual does not yet support the licensing mechanism of CODESYS Add-Ons. I assume that this is the reason for the error messages.
With ctrlX CORE hardware you can test the CODESYS Add-Ons in demo mode. In the demo mode the PLC task will stop after 30 minutes.
EDIT: ctrlX CORE virtual will support the licensing of CODESYS Add-Ons from ctrlX Store in version 01V18.
06-08-2022 02:13 AM
I have seen the same error when trying to run a SoftMotion PLC application on the virtual core (version 1.14).
11-17-2022 10:16 AM
ctrlX CORE virtual will support the licensing of CODESYS Add-Ons from ctrlX Store in version 01V18.