FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
06-14-2022 12:58 PM
Hello community members,
I am trying to use two CtrlX-Core as Ethernet/Ip scanner/adapter (eth1 port), I have to use the adapter on a project and use the scanner to test the adapter, I have read the document: "Installation Guide" and I have the licensens.
Any on that have a project example with the setup af both scanner and adapter?
Is the ethernet/IP running stable?
Solved! Go to Solution.
06-15-2022 08:45 AM
Am I right, that you are using the CodeSys fieldbus communication? Moved this topic to the corresponding forum.
01-16-2023 08:05 AM
Is this still an issue or can this topic be closed?