Solution Alternatives
Solution 1 - Update Device Admin
The easiest method is to simply update the Device Admin to version XCR-V-0120.7 or higher.
Update to Device Admin XCR-V-0120.7 (available in the Collaboration Room) or higher
Re-apply the license file of the device
(optional) Create a new setup file based on the new device state (for future use)
Solution 2- Adapt Setup
As an alternative to creating a new backup, you may manually update an existing Setup.
Download the latest Device Admin XCR-V-0120.7 (or higher) from the collaboration room (Device Admin XCR-V-0120.7.app)
Unpack the setup file and make following changes
Copy the Device Admin archive you just downloaded to the folder 'packageManagement'
Open the ctrlx-setup.json file and replace the information within the Device Admin (rexroth-deviceadmin) application section
Adapt the path under the rexroth-deviceadmin app entry to your previously copied binary name, e.g. "$path": "packageManagement/installedApps/Device Admin XCR-V-0120.7.app"
Change the version under the rexroth-deviceadmin app entry to the version of your previously updated application, e.g. "version": "1.20.7"
Add all files of the previously unzipped setup file to a new archive, e.g. "new_setup.zip" which can then be applied to your device causing the Device Admin application to be upgraded to the mentioned version
Re-apply the license file that was issued for the device (if not already included as part of the setup process)
The following screenshot shows an example:
hostid_mismatch
... View more