Hi, i created a snap with the C++ datalayer.register.node example and deployed it at a Virtual CtrlX. The node appears at the UI of the Datalayer and is also accessible. But sometimes the nodes disappear for 10-20s from the user interface of the automation snap. At this time, access to the node's url via other tools, such as postman, that were previously successful, are requested with a 404 error. After 10-20s the node appears and is accessible again. Is anybody facing the same issue or have a solution? I'm using the CtrX Works Version 1.2.2.
... View more