A project archive can be stored on the CF card via FTP when archiving a project. This must be consciously activated via checkbox ff. And if the project is later restored from there, and the compiler information and the IW version at the time of creation match the data in the controller, then you can also log in or be online directly. Conclusion: The project must first be stored on the controller (CF card).
... View more