The how to is more detailled than the documentation I got and seems to fix my problem. But it's not the device description I was looking for. I was looking for a json configuration file for the Profinet device configuration if you do not want to use a template: See this picture. I added the json as txt file as example. In that same picture, the state was Safe-OP (PROFINET Device v1.20.6), while the scheduler said it was OPERATING. (That will have to do that no IP-address or device name was set.) In ctrlX PLC Engineering the module does not show data in the status screen, but the data is availeble if I browse the data layer. For now it looks like I can proceed.
... View more