Hello Community, I have 3 different applications running on CtrlX core X3 with external USB as extended system data memory. 1st Application - InfluxDB from CtrX store: I have followed this guide https://developer.community.boschrexroth.com/t5/Store-and-How-to/IIoT-Use-ctrlX-CORE-as-a-monitoring-platform-using-InfluxDB-and/bc-p/81600#M746 It looks like, the setup is working fine and storing data. But yet to confirm, where the data is exactly stored - System data or sda1. 2nd Application - Container Engine App and one docker image(built and installed as snap). As far as I know and the knowledge gathered from forum, the docker prefers always the internal system data. So, the extended system data cannot be utilized really here. Please, correct me if I am wrong. 3rd Application - Custom snap with its files/folder mapped to appdata directory because I want to edit few configuration files during runtime. I guess, the appdata is part of internal system data only. Is there any possibility to keep or force this custom snap's files/folder to extended system memory and still make use of web UI based config file editing? Please, someone provide me general usecases where the extended system memory can be really employed and where not. Thanks & Regards
... View more