Hello! I'm trying to set up my CtrlX Core to be accessible over a WiFi network. I bought a USB WiFi dongle and plugged it into the USB-C port. It's showing up as another adapter under the connectivity settings. I immediately saw it show up on my router and assigned it an IP with DHCP which now shows up on the web interface. I can ping that assigned IP and get a response if I do this from the router but trying to do this from my PC or typing the IP into a browser to try to access the interface never gets a response. The CtrlX now shows that it has WiFi as well so it appears to be connecting fine. Is there some setting I have to do to allow connections over the USB adapter?
... View more