Nevermind, I finally got to solve it. What I noticed was when I updated the ctrlx PLC Engineering, what it did was it overwrite old library(the v1.12) making it corrupt and unreadable hence thats why the error/unidentified notification keeps popping up. After I uninstall and delete everything related to ctrlx works(the directory folder in C) and reinstall it, I finally get it to work as image shown below. Just incase if anyone got similar problem, What I did specifically are using uninstall manager>uninstall ctrlx works>opens <C:\Program Files\Rexroth> n delete whats left including the rexroth file folder>restart computer>reinstall ctrlx works v1.16>during installation, I didnt tick anything else other than the one it was defaulted>done installing, launch ctrlx works>launch ctrlx core webpage and launch ctrlx plc from it instead of from ctrlx engineering>once its launched, set all to newest and everything is now back online and good to go. (do note that project archive of plc ctrlx project program[default folder my Document] was being cleared 1st as in removed to another place just to be safe and do not do anything else while re-installing because sometimes it crashed and have to start all over again) Best Regard
... View more