Hello, I am currently using a web visualisation. It will show my visualisation on the following adress: http://192.168.2.10:8080/webvisu.htm. This is working fine. However, it will also redirect me to this page when I try to login into the main page of the ctrl x device. This is when logging in via ctrl x works but also when entering the ip adress of the device in the browser. The only way for me to enter the main paige is to stop the plc app (via ctrl x plc, i can access the ctrl x from here) and try again. This way I have no issue at all to enter the main paige. Once I have done this, I can leave the plc app (and thus visu) running without the issue of not being able to log in. So it seems it is only at startup. Is there any way to set up the ctrl x device in a way that this is no longer an issue? Thanks in advance!
... View more