Hello ! This post is related to the ctrlX DevelopR Challenge. I'm trying to write a python library to interact with the controller in pure python (so without the SDK which is a python wrapper). I also figured out the SDK only works on Linux systems (or Windows using the WSL) so that library could help to make the apps more portable. As far I could see, the SDK use the ports 2069 and 2070. Using nmap I figured out a ZeroMQ server is listening on these ports. I tried to snif the packets using Wireshark but the communication is encrypted with TLS (I found some funny words in there ... Maybe an Easter egg ?!) On GitHub, I didn't found the source code of the SDK. Any chance for you to release it ? Or could you briefly explain how the ZeroMQ communication works ? Which commands are sent for authentication and then to manipulate the datalayer ? Is the SDK used to obfuscate this part ? Thanks for reading, Regards Loïc
... View more