Hello @HmiGuide, I'm sorry, you're right, I should have put the post in the WebIQ section. There are two topics I am addressing here. 1. synchronous display on all screens. I use the Iq-resposive-menu and when a menu item is pressed, the respective menu content is displayed. (For example: Condition to show menu element -> setview -> Panel View [0] Home) Problem: Panel View Home is only opened on one screen and not on all screens. In comparison, I have a different behavior when I change the tabs in the tab panel. Here the tabs are switched synchronously on all screens. 2. recognizing which screen takes control. With conventional HMI applications, it was possible to recognize from which screen the system is currently being operated and to block or restrict the other screens. Is there a possibility to realize the same behavior with WebIQ?
... View more