Hello together, has someone ever tried to connect a Siemens PLC to a virtual CtrlX via the OPCUA_Client function block in Siemens TIA Portal? In the configuration of the client I can set up a connection to the CtrlX (only in TIA portal, not with hardware) but I can't connect the PLC via this function block. For the connection the function block uses the connection information of the configuration. For me it's weird because in the configuration it's possible to have access to the data layer but within the function block I always get the error message 8005_0000 within the subfunction OPC_UA_Connect (see screenshot). Would be so grateful if someone could help me with this issue! 🙂
... View more