03-12-2021 04:05 PM
Are there any plc functionblocks for the S20 I/O modules available?
In existing control platforms we are using the lib RIH_IndraControl_S20_XM for this.
Solved! Go to Solution.
03-15-2021 02:38 PM
Hello,
Yes, the lib CXA_S20, we ported, is available with RM21.03 v1.8.0.
The function block names remain the same, that existing code can be re-used.
03-15-2021 02:43 PM
Perfect, thanks for the answer.