cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

SFTP client connection with server

SFTP client connection with server

JLG_War
Established Member

I have an SFTP server running on a controller connected to the CtrlX. This server has a file that I want to read in the CtrlX with a python script. I want to create a SFTP client with node-red and store the file somewhere on the core preferable on the sd card. After the file is stored on the core I want to use a python script to read this file and depending on the content of the file do something with it. Is this is possible? I know the FTP topic is discussed multiple times on this forum but I couldn't found a clear answer so that's why I'm posting this. 

Thanks in advance. 

1 REPLY 1

TheCodeCaptain
Community Moderator
Community Moderator

Hi JLG_War,

there are several modules/paletts for Node-RED available doing an sftp connection, if one of them suits for you you can download the file.
See attached screenshot.

How to store it from Node-RED into the micro SD card you can find in this article:Solved: Re: Save a file created in Node Red on to CtrlX CO... (boschrexroth.com)

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist