08-10-2023 04:49 PM
ctrlX IO XB-EC-12 not connected state at EtherCAT master
An EC Device can be successful scanned and added, after activate&download the EtherCAT configuration to the EtherCAT Master with the crlX IO Engineering the EC Device appear as not connected. This is confusing. Because its present at the EtherCAT but not working.
I’m using v1.12 ctrlX Works and ctrlX IO Engineering with latest ESI files for ctrlX IO.
Solved! Go to Solution.
08-10-2023 04:52 PM
Issue is a revision mismatch between the ESI and the ctrlX IO XB-EC-12 bus coupler firmware.
ctrlX IO Engineering v1.12 cannot handle this two diffrent revision in the ESI, issue doesn’t happen with ctrlX Works v1.20.0 or later.
You have two options to solve in ctrlX Works v1.12
Both, the ESI package and firmware you can find in Downloads section.
08-23-2023 04:38 PM