05-02-2023 05:45 PM - edited 05-02-2023 05:47 PM
i have updated drive to 0316 and the core to 1.20 and am still getting a f8115 error on the drive
drive firmware shows to be 0316 and core was updated with the .tar, boot folder, rescue.itb file
i have tried multiple times and am getting nowhere, can someone tell me where i am going wrong
Solved! Go to Solution.
05-03-2023 11:20 AM - edited 05-03-2023 11:22 AM
So you are using a ctrlX DRIVEplus with integrated ctrlX CORE?
After updating both firmware (ctrlX CORE and ctrlX DRIVE) did you do a hard reboot of the drive (switch 24V off and back on)? Afterwards the error should be gone.
05-03-2023 05:19 PM
05-04-2023 07:23 AM - edited 11-14-2023 03:55 PM
OK, now the picture is getting clear. In your first post you mentioned control firmware 1.20 but you used 1.12.20 what is a big difference.
For that case you cannot use drive firmware 3V16 but need to use 3V08, as there is an internal interface between drive and control that needs to fit accordingly.
Fitting versions for actual releases:
ctrlX CORE | ctrlX DRIVE |
1.12.20 | FWA-XD1-AXS-V-0308N-NN.03 |
1.20.5 | FWA-XD1-AXS-V-0402N-NN |