FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
05-27-2024 09:20 AM
I am workign on a project which has an X3, SAFEX C12, ctrlX IO bus coupler+IO, then a Kistler Data Logger last on the EtherCat.
I can communicate to the C12 and IO with no problems. However, when I add the Kistler unit (using IO works, datalayer update and download) the EtherCat stops working at the ctrlX IO node. If I just have the Kistler unit by itself it works fine.
What could cause this? What information do I need to provide for someone to help me debug?
Solved! Go to Solution.
05-28-2024 02:51 AM
Can you try to create a new synchronization unit for Kistle to use.
05-31-2024 08:50 AM
Hi @JHU1XI1
I made a new synchronisation unit but that did not work. I was able to get it to work by putting the Kistler unit as the first device in the EtherCat daisy chain. This worked with or without a separate synchronisation unit.