FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
04-08-2024 04:22 AM - last edited on 04-08-2024 08:11 AM by HmiGuide
I'm using the Codesys Alarm Management system. When I add or change an alarm group message text is not updated until I do a Clean or do a full download and restart. Is this normal Codesys behaviour? Or something to do with ctrlX implementation of codesys.
Is there a way to update the table without doing a full download?
Start Situation
Change Message
Login the the PLC with Online change. The message still says "Hello". I tried rebooting the PLC but still no change. I tried deactivating and reactivating the alarm but the message does not change. I tried Reset Cold and Build-Generate code.
When I do a Build->Clean, or a Reset Original and download and start the PLC it changes.
04-08-2024 08:13 AM
I'm not familiar with the CoDeSys Alarm Manager, but I expect it works similar to other systems. Therfore I found thing article:
https://help.codesys.com/api-content/2/core_visualization/3.5.17.0/en/_visu_deleting_alarm_history/
04-09-2024 12:53 AM
Thanks @HmiGuide, However, I can clear and re-trigger errors, but the text does not change until I do a download.
04-15-2024 01:49 PM
Basically, there is no technical reason why this should not be updated with OC (onlinechange).
It just hasn't been implemented yet.
So at the moment there is only the workaround with the full download to use.
We are working on a solution and will try to integrate it into one of the next visualisation add-on versions.