So two weeks are enough time for official answer. I asked the same and it's like: Is it possible to run the IoT gateway software on the CtrlX core with the same functionality as the PR21? - No Is it possible to onboard PR21 to Device Portal, as long as we wait for ctrlX to close the gap? - No Is there any other way to get the same (sufficient for 95% of our usecase) functionality on ctrlX? - No, use Node-Red (a nice tool for quick prototyping), the "hey, almost 5% done"-Opc-Apps and develop everything on your own with the SDK So basicly BR ditched a working product with low effort for implementation, closing the gap for managed brownfield (and greenfield until development is done) IoT solutions without having something else in their portfolio.
... View more