There are ALIAS parameter available that can be written over SOE and these are following the 16Bit IDN.
In your case you have to use P2389 ad P2390 to be able to write S602.1.130 and S602.1.130. These are list parameters and you have to write the first list element to configure the physical encoder type.
Please refer to the parameter description of IndraDrive
... View more