There is a better solution, than using PLC Open XML format. Why?
Some code is changed and must be reworked after import
CoDeSys Visu, can't be exported/imported.
I use the following steps:
Unzip the IW project (e.g. myProject.xiwp)
With ctrlX Plc Engineering open <ProjectName>\Project\IndraLogic\IndraLogic.project e.g. myProject\Project\IndraLogic\IndraLogic.project
This project has the old libraries of IndraWorks, which means it can't be compiled and visu is not displayed correct.
To update the libraries the easiest way is:
Open a 2nd instance of Plc Engineering
Create a new project (this has the libraries of ctrlX)
Add the missing ctrlX libraries
With drag & drop copy the program and visu from the converted project into the new project.
... View more