Hi,
you can use any IP address of the drive which is reachable via TCP/IP from your pc.
A connection via panael/USB will always work - therefor you can connect to the IP address 192.168.222.x
If you want to connect via ET interface directly you have to disable EtherCAT communication. When EtherCAT is active you need to use at least a EtherCAT Master to establish a connection trough the control via EoE.
See also this how-to.
Best regards,
Christoph
... View more