Hi, Yes, indeed. Our first app (the current one) is a sensor (or data aquisition point) for Rhebos Industrial Protector solution. With this (almost free) app one may extend the visibility of an existing or a newly deployed Industrial Protector also inside the communication after the ctrlX platform. As an example from one of our customers: The ctrlX are used for production lines (or maybe better procuction/ machinery cells) which are also small networks, but with a good portion of industrial control communication inside. So it makes absolutely sense to monitor also thess network communication in such smaller network cells in the course of the comprehensive, bigger monitoring of all control communications in their OT network. A second app it is planned in future with a basic monitoring included already stand-alone without the necessity to connect this with the (bigger, and comprehensive) Rhebo Industrial Protector with its Controller and Sensors. It will give first insights regarding network quality and of course possible cyber security issues.
... View more