03-09-2023 09:02 AM
Managed to connect to the CtrlX core device, but i couldnt access to the PLC and ethercat configuration(as shown in the image), not only that, the "operation" tab is also gone. Then when i try to refresh the browser, i couldnt access back to this CoreX device. I can only connect to the device when i restart the CoreX device, but still getting the same Interface error(as shown in the same image).
Solved! Go to Solution.
03-09-2023 10:49 AM - edited 04-20-2023 11:24 AM
Could you please try to empty your browser chache (Ctrl + Shift + Del) and reload page then?
If this does not work please add a system report that can be created via the "About" or in newer versions the "?" symbol on the right top in your crlX CORE web UI.
03-15-2023 01:28 AM
04-06-2023 07:50 AM
Hello Wonder_Why
It seems you are using an older version. There the system report was found if you open the "About" screen.
Regards
Jochen
04-24-2023 09:05 AM
Is there still an issue or can this topic be closed?