cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

How to connect to a ctrlX CORE not shown in ctrlX WORKS or network folder

How to connect to a ctrlX CORE not shown in ctrlX WORKS or network folder

CodeShepherd
Community Moderator
Community Moderator

How is it possible to connect to a ctrlX CORE not shown in ctrlX WORKS or network folder without knowing its IP?

1 REPLY 1

CodeWasi
Occasional Contributor

Assuming:  - the ctrlX is not visible in ctrlX-Works or the Explorer/network and the IPsetup is unknown
                  - default setting of "enable DHCP" was not modified by the user in meantime

a reset can be avoided if a DHCP server assigns a IP adress to the ctrlX. Instead of placing a router HW to provide the IP-assigning there are several 'DHCP server for PCs available.

Exemplarily the following convinced by easy setup and handling.

https://www.dhcpserver.de/cms/running_the_server/

Installation and setup described in detail.

Once the dynanic adress was given by the DHCP Server, connecting the landing-page is possible and the static-IP adress can be adjusted once again.

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist