FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-21-2020 05:09 PM
Hello,
The function "Commond Axis…" or "ST code template" in context-menu is go away in CtrlX PLC,is there any way to run an axis conveniently ?
or will “Commond Axis” come back in the future? it's really helpful for new customers.
Solved! Go to Solution.
10-22-2020 10:12 AM
Hello,
to run an axis you have several options:
- Axis (Kinematic) Commisioning in the Web-Interface
- PLC AxisInterface-Projekt: Visualization "OverviewAxes" (OverviewKinematics) in folder AxisKinInterface
- PLC AxisInterface-Projekt: Sample code "PlcProg" and "DemoBufferedAxisCommands" in folder AxisKinInterface
There are no plans to implement "Command Axis..." and/or "ST code templates" by now.
I am not sure, if it is technical possible to implement this in ctrlX PLC Engineering.
10-25-2020 02:45 AM
What about "GAT"? Whether has a plan to implement it? Or whether has simmilar function in Ctrl-X?
12-02-2020 10:54 AM
At the moment (Version 01V06 RM20.11) there is an axis-, kinemtaic- and IMC-interface available.
See this thread for further information.
And GAT like known in the MLC is actually not prioritized.