cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

PLC project using the simple PLCopen FBs for 3 axes / 1 kinematic (="Robot")

CodeShepherd
Community Moderator

PLC project using the simple PLCopen FBs for 3 axes / 1 kinematic (="Robot")

Is there an example commanding a kinematic via PLCOpen function blocks out of the PLC?

1 REPLY 1
st_ctrlX_user
Long-established Member

PLC project using the simple PLCopen FBs for 3 axes / 1 kinematic (="Robot") for free :-) if needed

This is not a question, it's just an example of a PLC project for 3axes/kinematic as well with real axes as with COREvirtual.

If someone needs a ctrlX plc-project showing the PLCopen function blocks for moving a kinematic, reset and also switch EtherCAT state and see status of PLCopen state and EtherCAT-state please find attached the ctrlX-PLC-Engineeering export file and fill free to contact me if you have questions. A short movie is also enclosed to see how to use my small internal visu.

I didn't use the much more comfortable allready existing AxisInterface in this project. It's just to see how the functions "Add Axis to Group" and "GroupEnable", "MoveLinearAbsolute" work together.

For myself I din't know before that the command MC_AddAxisToGroup has to be used.  I thought GroupEnable is enough 😉

Regards, Stefan Svoboda

Tags (1)
Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist