cancel
Showing results for 
Search instead for 
Did you mean: 

Leave AH mode error - 090F2002/0C570100

Leave AH mode error - 090F2002/0C570100

Xiaoyin
New Poster

I used the Axisinterface modular for test. The core is  'X3 and drive is ctrlx drive (xcs)'.

The axie can  execute the position moving or velocity moving normally. But everytime when leave the 'ModeAH' command, the error appeared, meanwhile the servo stayed in AF state. The error can be reset. But why this error appeared? How to solve the problem?

Pls refer the pics for details. error.pngcommand.pngplc_version.png

apps version.png

4 REPLIES 4

CodeShepherd
Community Moderator
Community Moderator

As there are several improvements made for such errors in the latest version please use the current release version of the ctrlX PLC Engineering 2.6.5 as well as ctrlX MOTION app 2.6.6 and check again.

Thank you for reply.

The newest version of 'motion app' is 2.6.5. How could I get the 2.6.6 version?

2_6_3 APPS.png

CodeShepherd
Community Moderator
Community Moderator

It can be found in the official ctrlX Store page

EDIT:

Only the text in the app package in the early adopter area was incorrect. Now the correct version 2.6.6 of ctrlX MOTION is mentioned.

Hi,

I'm using Motion App 2.6.6 & PLC Engineering 2.6.2.

And I'm having the same issue, but for me the error is not resettable (even from plc, DL or webserver).

Also, I'm not able to command the axis's mode (it's stuck in AH).

I've already tried to avoid changing the OpMode if the axis is stopping or stopped (AxisStatu.Data.PlcOpenState.stopping), it solved a lot of cases, but this error sporadically pops out and I'm not able to control the axis.

Regards,

GB

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist