FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
09-07-2021 10:02 AM
Which tags are typically used in the ctrlX MOTION forum?
Solved! Go to Solution.
09-04-2021 09:44 AM - edited 02-16-2024 01:05 PM
Please do not delete this post. It is necessary to tag the posts correctly and not with similar but different tags.
Tag list part 1 (a-h):
3ddemo, 3dviewer, adapter, addons, axes, axisinterface, axisprofile, axssetipoposfromactpos, backup, blending, booting, buffer, c++, c_programming_language, cam, cam designer, cartesianrobotics, ccd, ci(_customer issue) , cycletime, cnc, coe, command, continuousslope, controller, controller2controller, csharp, ctrlxcorevirtual, ctrlxdrive, ctrlxio, ctrlxmotion, ctrlxplc, ctrlxsafety, ctrlxworks, customerrequirement, cxa_driveutil, cxa_ethercatmaster, cxa_loopcontrol, cxa_motioncore_fbs, cxa_motioninterface, cxa_plcopen, cxa_python, cytrobox, cyclicsetpoint, cytropac, datalayer, debug, delta, deceleration, deltarobotics, device, diagnosis, dihighspeed, dioversampling, direction, ditimestamp, documentation, dohighspeed, dooversampling, download, drive, driveconnect, drivecontrolledhoming, drivecontrolledpositioning, driveinternalinterpolation, drivelink, e-stop, electronicgear, encoder, engineering, error, errorcode, errormessage, errorstate, errorstop, estop, ethercat, ethernetip, euromap67, fixed stop, flatbuffer, flexprofile, functionblock, fx (opcua, fx), gantry, handling, halt, hardwareexchange, hmi, homing
10-27-2022 08:22 AM - last edited 3 weeks ago
Please do not delete this post. It is necessary to tag the posts correctly and not with similar but different tags.
Tag list part 2 (i-z)
ide, imcinterface, indradrive, installation, kinematic, kininterface, license, licensing, licensing center, limits, linuxcnc, logbook, manual, master, Maxon, mc_movevelocity, measuring wheel, mlc, mld, modulo, motioninterface, moveabsolute, mpb, mpc, mpe, mtx, mtxmicro, newest-version, node-red, offline, omac, omron, opcua, operationmode, oversampling, packml, paletising, panasonic, parametrization, parking-axis, performance, plccontrolledaxis, plcopen, polytrans, position-mode, profinet, project-conversion, python, q&a, realtime, registercontrol, release, reset, rest, restore, rm2011, rm2103, rm2107, rm2111, rm2203, rm2207, rm2211, rm2303, rm2307, rm2311, rm2403, rm2407, s20, safearea, safetorqueoff, safex-c.12, safex-c.15, safex-c.1x, sample, scanner, script, scheduler, sdk, setup, sfk, sfk4h, slave, snc, somo (synchronizing motion objects), startup, steppermotor, sto, synchronization, synchronizing_motion_opjects, syncmotion, syncunit, sytronix, task, tcp, tempcpu, Temperature, template, tensioncontrol, timestamp, timing, torque-mode, touchprobe, training, update, v112, v114, v116, v118, v120, v202, v204, velocity, velocity-mode, virtualaxis, visualcoding, warnings, winder, workingarea, workshop, write, x3, x7, xinje, xm, xm2, xm21, xm22, xm42, xvr
01-23-2023 01:18 PM
Hello Michael, it is a good idea to have such a Tag list, but please don't use any underscore and keep the tags as short as possible.
Example:
Thanks & Regards
Katja
02-16-2024 09:30 AM
Hello @KatjaX , which tag would you suggest for "OPC UA FX" (see)? I read the "Guideline for creating an article" and found the hints:
Thanks, Michael
02-16-2024 12:53 PM
Hello @MichaelB,
Thank you for your message.
For OPC UA FX I would suggest following tag: "opcua, fx".
It's better to create 2 tags. One for "opcua" and another tag for "fx", separated by a comma.
Hope this will help.
Greetings, Katja