cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

MC_ReadActualVelocity and MC_ReadAcutalTorque

craigthomp
Established Member

MC_ReadActualVelocity and MC_ReadAcutalTorque

What is required to get MC_ReadActualVelocity and MC_ReadAcutalTorque to operate?  In my testing they always return 0.  Is there a way for these function to read S-0-0084/S-0-0040 configured in AT so they update the data cyclically.

3 REPLIES 3
Jochen_Mueller
Community Moderator

Re: MC_ReadActualVelocity and MC_ReadAcutalTorque

No, it is not possible to get these data at the FB by configure the two parameter at the AT.

The FB will read Motion-App internal values. Some are already "connected" to the drive parameter (via AxisProfile), some not (e.g. velocity, torque). With the implementation of further operation-modes this "connection" will be done.

For the velocity this will come with the next RM22.03. For the torque sometime later.

bschmidt
Long-established Member

Re: MC_ReadActualVelocity and MC_ReadAcutalTorque

For now, as you probably know, you can read as I/O via the DataLayer then convert to REAL. But it will be more convenient to have this data already available via the Axis Profile. 

bschmidt_0-1642430062294.png

bschmidt_1-1642430108547.png

 

 

MichaelB
Community Moderator

Re: MC_ReadActualVelocity and MC_ReadAcutalTorque

Velocity mode is now available with RM22.03 (V1.14).

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist