FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
03-07-2023 09:40 AM
Hello.
What could cause this behavior?:
The status Led is solid Red in the EtherCat Bus module always after power on. Both Up and Ul supplies are connected and I can monitor the voltage. Only when I disconnect Up and connect it again the Led changes to green. There are no diagnostic errors in the module when the led is red.
All the IOs are green as they should.
Solved! Go to Solution.
03-07-2023 05:32 PM
wrote a PN to clarify, than we'll update the thread
11-13-2023 03:39 PM
Are there any news and/or can this topic be closed?
11-16-2023 01:54 PM
This can be closed