I/O Engineering - Slave to Slave connection can't be saved

I/O Engineering - Slave to Slave connection can't be saved

MST
Established Member

Hi everybody,

I'm trying to connect EtherCat Slaves via the slave to slave configuration in the I/O-Engineering (V1.20.1). It works e.g. for the connection between SICK Sensors and the SAFE-X configuration:

2023-10-17_15h04_50.png

I can download the configuration as shown in the picture without any problems.

As soon as I add any connection using the KRC4_secondary_EL6695_1001 slave (example in the picture below)...

2023-10-17_15h05_35.png

... and download or save the project, the configuration is deleted (see below).

2023-10-17_15h06_18.png

It is also deleted, when the configuration is made offline without any conecttion to the EtherCat (Cable unplugged). Therefore I don't think it is overwritten by any other participant in the network. Any idea where my problem is? The communication between the Kuka-Slave and the PLC-App works fine and data exchange is possible. Also the ESI-File is the latest from the KUKA downloadcenter.

Thanks for your help and regards 🙂

3 REPLIES 3

CodeShepherd
Community Moderator
Community Moderator

Could you please provide us the device description files you are using? Especially the KRC4.

MST
Established Member

Attached, the description files I use in the project.

For your Info, I got the KRC4 file from the KUKA download center:https://kuka.sharefile.eu/share/view/s7ecbfd0b091f477d88bac2c865f09a3d/fof1a212-aa67-4e34-995b-2b03e...

jacaré
Long-established Member

This issue is known and is fixed with the Version 2.02. For the Version 1.20 it will be fixed with the Release Milestone 24.03 (2024 March)

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist