cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

WebIQ IO Manager

WebIQ IO Manager

Tamer
Established Member

Hi,

Has anyone had any luck establishing communications between ctrlX core virtual and the WebIQ app? I am trying to create a new entry in the IO manager to communicate with the OPC UA server on the virtual core, but I get "Error adding IO handler, (Error code:3, category: shmi connect:api:io_extension, message: failed to load).

I have set the Endpoint URL on WebIQ to 'opc.tcp://localhost:4840', and changed the certificate to trusted on ctrlX core. The user (boschrexroth) full admin and OPC-UA, has full permissions.

Any feedback would be highly appreciated.

5 REPLIES 5

stefanAT_ctrlX
New Contributor

Hello Tamer,

yes, I've done. But it took me also many hours 😉  I don't know which mistakes I did. But it's working. I just tried again. Here are my adjustments:    Yes, as you wrote, to trust the certificate in the CORE (Virtual) was necessary.

st_ctrlX_user_0-1616422280697.png

Regards, Stefan

Hi Stefan,

Thank you for your response.

I tried using same inputs as in your post, but it still did not work. I am not sure if the namespace (http://www.boschrexroth.com/OpcUa/Datalayer) is the right one? I also tried to copy the link of my own PLC global varaible list I was trying to link to (ex: https://localhost:8443/automation/datalayer#plc/app/Application/sym/GVL) but with no success.

I also can not see the OPC UA permissions included when I open the session details after failing to connect.

Tamer_1-1616456175703.png

 

 

I think you checked with an OPC-UA client e.g. "Unified Automation UaExpert" the namespace ?

In my example:

st_ctrlX_user_0-1616486461744.png

Then your namespace should be the right.

At ctrlX CORE virtual I use port forwarding with adjustments: 8022:22,8443:443,8740:11740,4840:4840,10123:10123

 

 

Thank you Stefan.

I do not know why, but it only worked when I copied the Namespace from the UA test client, perhaps I missed a character.

Tamer_0-1616545759971.png

 

Is there some detailed information avaible somewhere on how to connect the UPC UA server to WebIQ and te CORE? I am waiting or the server app so I can easily communicate with the CORE using the webIQ. a good alternative is the OPC UA server but I have virtually no experience with this so some documentation and explanation would be nice.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist