Kiosk Mode for Panel PC

Kiosk Mode for Panel PC

Hemingway
Established Member

Hi, do anybody has approach how to autostart webiq HMI on PC panel at kiosk mode? Now, I am trying to write vbs scrypt which open Chrome at Kiosk Mode from shell:autostart but it looks week. 

5 REPLIES 5

HmiGuide
Community Moderator
Community Moderator

Just from the internet. On PC chrome has the start option -kiosk. So create a shortcut with the options described below and place it in Windows Autostart, if required.

You can use any website in the following command: “C:\Program Files (x86)\Google\Chrome\Application\chrome.exe” -kiosk https://praxistipps.chip.de/ --overscroll-history-navigation=0
Google Chrome only starts in kiosk mode if no other Chrome window was previously open. To exit kiosk mode, use the key combination [Alt] + [F4].

chris-p
Established Member

Hi @Hemingway ,

Our Windows-based IPCs and HMIs have the “Shell Launcher / Custom Shell” feature. Here it is possible to start a specific program (Chrome in the example) with a parameter at startup. The desktop or similar is not loaded first, but only the selected program.

If help is needed or there is interest, I can provide a few examples.

Hemingway
Established Member

Hi, @chris-p ,

Yes, please provide some examples. 

chris-p
Established Member

Hi @Hemingway ,

here are some example files. Feel free to contact me if you have further question.

webiq-sk
Frequent Contributor

You can simply use our free Electron Kiosk Browser Builder you can download from https://www.smart-hmi.com/user/download/deliver/xmp/Additional%20Software/webiq-kiosk-browser-builde...

This will build a customized Chromium-based browser using ElectronJS and it will also automatically reload your HMI in case an error occurs.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist