FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
01-31-2024 09:09 AM
Hello,
I have a customer who like to use pipeline animation.
He wants to animate the flow of water in the (pipe)line, for examle with moving dots in the direction of the flow.
Is this possible in one or more ctrlX HMI app(s)?
Regards, Mike
Solved! Go to Solution.
01-31-2024 04:05 PM
The WebIQ Animation Demo shows an example: https://demo.smart-hmi.com/demo-animation/
01-31-2024 04:32 PM
07-16-2024 12:04 PM
Hello there
It is possible to use ctrlX HMI apps to create a pipeline animation that replicates the flow of water by using replacing dots. This can be placed into effect by producing a unique animation that represents the flow of water through the pipeline. When interacting the direction and speed of the flow; fluid characteristics such as a flowing line and moving dots might be used. You can add this animation into your user interface to give real time feedback on the operational state of the pipeline due to the flexibility of ctrlX HMI.