Back to forum overview
Something went wrong
Latest / Featured posts
Featured
No posts to show here
Posts
WR21 keyboard too large
Is there some calibration for the size and scale of the WR21? What I am seeing is that points that you touch are off from the keyboard and the keyboard itself hangs over the edge of the screen. For example, the "p" button has to be pressed in order to hit the backspace. I have images but cannot upload for some reason. 001/22/2025WR21 Factory Reset
I have a customer who has locked their WR21 after too many incorrect password attempts. I'm assuming the only way to recover from this is to reflash the panel, as described in section 3 of the software manual. I have not been able to find the image file called out in the manual. Can anyone help with the location of this file? Or is this something I need to request through a different channel? 201/16/2025Could not establish connection between ctrlX OPC UA Server with Helio
I tried to connect Helio PLC Data with my ctrlX OPC UA Server, but the connection could not be established when I started the test. Is there anything I can do? 1001/06/2025ctrlX HMI real time clock not working
Hi Community, I have a ctrlX HMI whenever restarted the date/time will lose the real time time clock. Anyone had this issue? Warmest regards, 112/26/2024Boot Ubuntu on WR2110 Panel
Has anyone successfully booted a WR2110 HMI into Ubuntu from an SD-Card? According to the Manual from Advantech (manufacturer of the Panel), this should be possible -> see attached picture down below. Sadly I'm unable to locate the needed pre-built Image. Advantech refuses to help me because I'm working with a rebranded rexroth unit... 012/19/2024Button to enable velocity change
Hello, I'd like to write in an input field a new value for a PLC variable, but I'd like it to not update the PLC variable until I press a button. So used an input field widget linked to a internal variable and a button which should write the value of the internal variable to the PLC one. But it seems not to work. Could you please help me? I've tried to attach other screenshots of the widget and the variable but it seems I can't 1712/11/2024CtrlX HMI scroll issue on chromium - Smart Function Kit
Hello, We are using SFK4P and we'd like authorized personel to use it from station PLC's HMI. Issue is, as far as we see, kiosk mode only works for one website. We cannot add second kiosk or second webstation app to kiosk so they can switch between WebIQ and SFK dashboards. So, we thought we could use chromium for SFK dashboard. Problem is, we cannot scroll on SFK page. It just doesn't work. We cannot see live values or if you are logged out, cannot log in because button is on bottom left and we cannot see it. Do you have a solution for that? Changing website address of kiosk's webstation settings is not user friendly so customer doesn't want to do it. We are open to suggestions. Thank you for your support. If forum goes read only and if messaging works, you can contact me via DM too. It's really appreciated. 311/22/2024Shifted Android frame at WR Panel
Hi, I have a strange situation with WR Panel, looks like the whole frame shifted to the top. Did you ever encounter suach a situation. I've tried to reinstall RC4, but it doesn't work. 111/22/2024Recommendation tablet model
Hello, A customer asks me for a recommendation for an industrial tablet model. The machine is large and the WebIQ project would have about 700 Tags. The client wants it to be industrial (case reinforcement, extra battery, etc) does not want to use domestic. Someone could recommend me one. Thanks. 211/08/2024ctrlX HMI - Basic Template - Online training possibility?
Dear All! Is there any way to get a short training about ctrlX HMI - Basic Template usage? We would like to understand deeply the PLC template+WebIQ template connections, especially the table-manager and recipe handling features! Thank you in advance! 210/17/2024ctrlX HMI Ethernet port data missing
Hello, Sometimes at startup the ctrlX HMI dissapears the Ethernet port information. From: To: It is need to configurate again. Why is this happening? Hardware: WR2107.1-111-AA-000-NN-A1-NN Thank you in advance! 109/20/2024Setup WR21 with Codesys WebVisu
Hi, I’m new to PLC programming and am currently trying to design an HMI using Ctrlx Codesys and Webvisu. I have obtained the Webvisu license, but I cannot find any documentation on how to display the HMI or set up the WR21 with the Ethernet port for display. Can someone assist me with this as I am a complete beginner? Additionally, I encounter an error when I run Webvisu on my local machine. Any help would be greatly appreciated. 909/16/2024webwiew app not installed
Hi I already installed RC7 update un WR21, but webview app is not installed in kiosk mode (see attach) how can install it to open hmi app in kiosk mode 109/06/2024Webpanel SSL certificate authentification failed
Hello I programed an application in webiq software, Webiq server is already installed in Corex X3, i configured Kiosc mode in Webpanel WR 2110.1-111-AA-000-NN-A1-NN. Before app started security warning is displayed (see attached pic). Does Exist any easy way to eliminate this alarm? 109/05/2024WebIQ does not connect with OPC UA Server
Hi, we are working on a Projekt for controlling a robot with a CtrlX Core. Unfortunately, there is a problem with the connection between the WebIQ and our OPC UA server, running on CtrlX Core. All certificates and licenses are instaled and active. The error shows in the WebIQ-Designer in the IO-Manager as "waiting_for_reconnect" (screenshot atached). We already checked the Port and IP for the communication. The Variables are currently shown, but while running the WebIQ-Projekt, they are not set in the CtrlX Core program. (WebIQ-Runtime and -Designer Version: 2.15.9) Questions gladly Many thanks in advance With kind regards 508/09/2024APK file for WR Kiosk
Hi, do we have an apk. file for Android Kiosk from our Standard WR? A have to check this kiosk on Samsung Tablet. 307/31/2024Kiosk Mode for Panel PC
Hi, do anybody has approach how to autostart webiq HMI on PC panel at kiosk mode? Now, I am trying to write vbs scrypt which open Chrome at Kiosk Mode from shell:autostart but it looks week. 507/18/2024Adding certificate to Chromium WR21
How to add certificates and open https page on Chromium Android WR21 without information about your connection is not private? 407/17/2024WR21 Browser does not support WebGL - Virtual Assist
Using WR21, updated to RC7, load WebView as well. Chromium shows a message that WebGL is not supported by the browser when trying to open Virtual assist, same error on WebView app. Enable hardware accelerator on Chrome and did not help. Any assistance will be appreciated. Thanks 306/05/2024HTML Page Autostart on Android
I've created a simple html page which open webiq project after some offset. On my local PC everything is fine. The question is how to insert this .html file into WR21, and how to autostart this file after WR21 has rebooted? 503/27/2024auto refresh timeout on startup of WR panels not working
Today I updated my WR15 to RC7 and tried to delay the start using the setting on the URL page for Kiosk mode. The screen now tries about 20 times to establish the link. But this only takes about 30 seconds. X3 takes about 3 minutes to boot. So the browser just faults to 404. See video attached. Is there something I am missing? 703/26/2024VPB equivalent with ctrlX
In VPB40.4, there was two display port, CDI & DP. And it was possible to connect monitor directly on Display port and another ctrlX HMI DE ( R911404268) on CDI+ port. And so external monitor was only used for monitoring and HMI was used for machine operations. How can we do similar configuration with ctrlX CORE or ctrlX IPC?? 403/15/2024Problem with WebIQ Trend on WR21
Hello, I have the issue that WebIQ Trends showing up different on two different devices. The server runs on a CORE X3. On the picture attached I had connected a laptop (the trends look how they should) and a WR2110 (the trends look faulty). On the WR21, the trends are not shown historically but show the actual values over the complete time interval (e.g. 1 minute, no affect of changing the interval). There is a different behaviour in some other points too: When unchecking and re-checking some trends via the Trens Select on both devices, the y-axes are grouped the way initially defined only on the laptop, not on the WR21. In case I only selcet one trend to be shown, the laptop shows one fixed y-axis and the moving trend. On the WR21 the trend remains in the middle of the widget and the y-axis is moving instead. Setup: X3 with 1.20, WR2110 RC7, WebIQ 2.15.7 (both, designer and server). The devices are offline but time is synchronised (on CORE via browser, on WR21 manually). Any suggestions from you on how to fix that issue? 502/22/2024HMI Pipeline animation
Hello, I have a customer who like to use pipeline animation. He wants to animate the flow of water in the (pipe)line, for examle with moving dots in the direction of the flow. Is this possible in one or more ctrlX HMI app(s)? Regards, Mike 301/31/2024WR21 was reset by itself
Hello Community Fellows, A customer of us had a problem that WR21 stopped working. I had a look into it and found at both the webIQ project was not available in the ctrlX Core, some how removed, and also no IP address was found in the settings. According to customer they did have some power breakdowns becuase of groud problems in the cabinet. Have anybody experience with this? what can be the reason for this? Regards Babar 101/17/2024WR21 cannot update to RC7
Hello, I have a WR2115 that I had succesfully upgraded from the RC2 to the RC4, However now I have downloaded the RC7 from the website and using the same procedure as before it is not working, If i enter the OTA.apk and I press on "Update" it shows us like a progress bar that stops at 1% or 5% and then automatically the OTA.apk and this progress bar pop-up fade away and I go back to the starting menu Sometimes it returns this error, I have also tried to power off and power on the screen and same result, I have also tried to upgrade the OTA.apk application, because maybe it was different between the RC4 and the RC7, but same happens, Does anyone have experienced this? How can I solve it? Many thanks, 512/20/2023WebIQ not working in CtrlX HMI WR2107
Helo, i have facing issue with CtrlX HMI WR2107 and WebIQ HMI. I create a WebIQ HMI and upload it to WebIQ Runtime in CtrlX, when i try to access the HMI using tablet, smartphone, and laptop everthing is fine. But when i try to access the HMI using CtrlX HMI WR2107 it's appear like this Using HMI default browser Using Chrome Browser is there anyone here who have same issue? 412/04/2023Howto run Chromium browser in full-screen mode on WR web-panels
Howto run Chromium browser in full-screen mode to achieve kiosk-like view on ctrlX HMI using Rexroth WR20x, WR21x web-panels? 511/08/2023SSL certificate authentication failed, continue loading?
SSL certificate authentication failed, continue loading? -error message appears during the boot of the core with webiq server installed. Is there a solution where to set the ssl? Please advise. 1511/07/2023CRASH KIOSK APP WR21 with Codesys WebVISU
Hello, we've a customer using a WR2107 (FD : 23W09) as a panel for Codesys WebVisu, the application is very very basic, but we are getting a crash of the KIOSK App at least once a day! do you have any information about that ? KIOSK SETTING APP Version : V1.0.6. @Nathanael for info 410/25/2023Web Station - Security Warning
When initially accessing a WebIQ visualization on a WR21 panel via the Web Station app a security warning will display. I believe this is casued by a certificate issue, which is discussed in this post. Unfortunately, there doesn't appear to be any way to eliminate the warning by importing a certificate into the Web Station app like you can with Chrome. Is there some method to bypass this that I'm not aware of? If not, are there plans to address this in subsequent versions of the Web Station app/panel firmware? 610/20/2023Multiple button control
Hello, Is it possible for hardware (e.g. Rexroth screens) and software (e.g. WebIQ) to perform two actions at the same time by pressing two individual buttons? So, like the example below, the buttons to run the motors should be able to be pressed to run the motors individually AND also at the same time. For example: press button 1 to run motor 1, press button 2 to run motor 2 (at the same time), release button 2 to stop motor 2, release button 1 to stop motor 1. Regards, Mike 210/12/2023File Access in Kiosk Mode
I have a WR21 panel that is running in kiosk mode and connected to a WebIQ visualization hosted on a ctrlX Core. The visualization uses WebIQ's integrated recipe handling, which includes importing and exporting recipe files. This process works fine on the panel's Chromium browser but not in the kiosk mode web viewer. Is this the intended functionality of kiosk mode? I understand the necessity of locking a user out of most OS functionality but I expected file access would be possible, albeit in a more limited manner(maybe just to the 'Downloads' folder?). If this isn't intended, is there a timeline for adding file IO support for kiosk mode? 408/31/2023Spare Parts for WR21 (R911411946)
I am needing spare parts for the WR21 HMI. Seems to have misplaced the panel clamps for installing it and I do not see a part number listed in the manual. Distributor was also not able to find the part number. 308/22/2023High Rexroth resolution GIF
Hello Are the Rexroth A Bosch Company and CtrlX Automation GIFs which are just above available in high resolution ? 107/12/2023Incorrect input when the screen saver is active.
Hello, When the screensaver is activated, the screen is dark. The user must tap the screen to disable the screensaver. When deactivating, a function / key (e.g.: system on) is activated. How can I prevent accidental tapping of a key when disabling the screen saver? 206/26/2023First Use WR21 and WebVisu
Hopefully some nice easy questions... My first use of WR2107 and WebVisu (do not have hardware yet so unable to test before developing screens) and haven't found much documentation so please could you answer the following: 1. WR2107 screen resolution is 1024 x 600 so was going to develop WebVisu screens in same resolution. However do I need to allow for any space for browser frame/window or is it possible to launch browser without border? 2. How would you configure browser to auto start to correct webpage on power cycle? 3. What browser is installed on WR2107? 4. Any other configuration hints? Many thanks! 306/22/2023
Latest updates on forums/articles
- 284 posts
- 114 posts
- 334 posts
- 147 posts
- 74 posts