05-05-2020 03:58 PM
Is USB-C interface, correct? Or is there a microUSB available?
Solved! Go to Solution.
05-11-2020 08:23 AM - edited 05-11-2020 08:26 AM
In a ctrlX CORE standalone an USB-C connector with USB2.0 speed is available. Actual no communication can be done there.
In a ctrlX DRIVEplus witch ctrlX CORE there is no USB on board. You will have to attach a panel for this functionality. Actual only communication to the drive is possible.
05-11-2020 02:04 PM
Yes, that´s true! It is a USB-C interface present on the panel only.