FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
08-04-2022 01:48 PM
Is it possible to use the multiplex channel functionality in Ctrl-X as in Indraworks.
I would like to read and write PBM-parameters to the drive with the multiplex channel function.
Is this possible and if so, how and where can I configure the multiplex channel configuration?
Solved! Go to Solution.
08-05-2022 01:09 PM
Yes, this is possible. You enter the data in the parameters S-0-0370 or S-0-0371 and see them in the master communication settings. See: