cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Ctrl X Drive 2 axis synchronization for gantry application

Ctrl X Drive 2 axis synchronization for gantry application

GBARyder
Member

Is it possible or when wil this functionality be available?

Synchronization of 2 axis in  a gantry application

Complete solution is made up of 2 synched Z-axis and an X axis mount between the 2 z -axis as per enclosed 

Controlled by control X core

2 REPLIES 2

Drives_Uwe
Community Moderator
Community Moderator

With the motion app of ctrlX CORE this functions already quite a long time. The Gantry function inside the motion app synchronizes the two Z- axes.

Alternatively in future the ctrlX DRIVElink function will allow to realize this only based on drive functionality in order to avoid the motion app. Means then only the PLC app would be good enough. This function will be available by end of 2022.

MichaelB
Community Moderator
Community Moderator

see here the documentation of the ctrlX MOTION functionality

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist