cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Cannot Power- up my second ctrlX Drive (XMS) in the Ethercat topology

Pinball_NL
Long-established Member

Cannot Power- up my second ctrlX Drive (XMS) in the Ethercat topology

I tested the demos set of ctrlX (with core) sebveral times. This worked out faultless.

I placed and scanned a second Drive (Indradrive Cs) in the Ethercat ring, scanning / running worked quit easy.

When I used a second ctrlX (XMS without Core) as a second axis. Comissioning worked out fine till I hit the power command in the comissioning. Here I get an error and I could not get this axis running.

I had to go online with ctrlX-Drive software and found this axis not going from bb to Ab. I pushed the green button (you hear the relais) but internally the drive does not go to Ab ! Thus you cannot power up.

This is different with Indradrive Cs. When you put 230/400V on a drive in bb, it goes automatically to Ab. But beware ! We have a ctrlX drive here which is powered over the DC-bus. This drive is not going automatically to Ab when the DC voltage is present.  You have to configure this over a input or over Ethercat. A master control can check the status of the power supply and (all) the ctrlX drives and give the signal okay (switch to Ab)

So if you have a ctrX drive just for testing you have to set this manually ! Depending how you want it, you can arrange this.  But the easiest way is to set P-0-0118 (bit 15). Then the drive goes to Ab when the DC bus is present (check the voltage). This is for internal test purposes only.

 

 

2 REPLIES 2
DepecheMode
Established Member

Re: Cannot Power- up my second ctrlX Drive (XMS) in the Ethercat topology

Please refer to the project planning instructions R911386579

DepecheMode_0-1603195568211.png

On page 107 you can find an example of wiring via I / Os

DepecheMode_2-1603195761381.png

 

 

 

CodeShepherd
Community Moderator

Re: Cannot Power- up my second ctrlX Drive (XMS) in the Ethercat topology

See here a link to the online documentation.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist