cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

NodeRED RED-V-0204.0+3.1.0-ctrlx does not start when using a proxy

NodeRED RED-V-0204.0+3.1.0-ctrlx does not start when using a proxy

CtrlXplorer
Established Member

Hello everyone, I encountered the following issue:

Used software :

  • ctrlX CORE Virtual image version 2.40
  • NodeRED RED-V-0204.0+3.1.0-ctrlx 

After enabling the proxy tool (Px.exe) and configuring the proxy settings (ctrlX Core Virtual -> Settings -> Proxy) NodeRED web app displays the message:  The app is currently not available. I waited for 10+ minutes, refreshed the page but I got the same message.

However, when I disable the proxy settings (ctrlX Core Virtual -> Settings -> Proxy). NodeRed starts flawlessly. However, since I am connected to a corporate WiFi network, I do not have any internet access in the ctrlX Core.

Note: I managed to resolve the issue by downgrading to a lower version of the:

  • CtrlX Core Virtual image version 1.20.9
  • NodeRED RED-V-120.0+3.0.2-ctrlx

 

23 REPLIES 23

MauroRiboniMX
Contributor

Hello,

See, we were able to reproduce, we will open an internal ticket to fix this 🙂

PS i tried with the image 2.04 and node-red 2.2.0+3.0.2-ctrlx and is also working! so i think we have to check what is new in node-red from this point of view 🙂

MauroRiboniMX
Contributor

did u check also with 2.4 image and node-red version 2.2.0+3.0.2-ctrlx. FOr me is working, can you check on your setup please? 😁

Hi,
sorry for the late reply. I just tested your mentioned configuration 2.4 image and node-red version 2.2.0+3.0.2-ctrlx and I can confirm that NodeRED starts sucessfuly. 🙂

We are working on a more clean way to start node-red with the proxy for the next releases 😁
meanwhile i don't think that makes really a huge difference to use this or the other version!

 

Got it, thanks for the update! Closing the ticket now. 🙂

Where did you download that NodeRED version of the app "node-red version 2.2.0+3.0.2-ctrlx"? I only found the "Node-RED 2.4.0+3.1.0-ctrlx" with the image "2.4.0" from collaboration rooms. The CtrlX can connect to the Internet as the proxy is already running, but cannot start NodeRED app...

cal9mx2_0-1718398749528.png

cal9mx2_1-1718398773030.png

 

 

CodeShepherd
Community Moderator
Community Moderator

@cal9mx2 please check out latest version "Node RED RED-V-0206.2+3.1.7-ctrlx"

@MauroRiboniMX did you test the latest version already?

Affermative 😊. Should be solved from 2.6 this issue

 

Bobby
Established Member

Hi,

Same issue happening to ctrlX virtual base image version 1.20.13 with node-red. And my ctrlX works not able to get the older version image. How to resolve this?

Hello, 

Which node-red version? 😀. I give a look today again 

Bobby
Established Member

Hi im using this version,

Node RED RED-V-0120.2+3.0.2

Should be solved in the next release with 2.60 release, end of this month

Bobby
Established Member

But i am using image version 1.20.13. it cannot use version 2 apps right?

Hello, 

No but technically should be fixed in the nex version, i have to check with developers. I think you are doing a connection for PX proxy right? 

This setting is solving the issue 😁. Meanwhile we check with the devs when the fix is coming

MauroRiboniMX_0-1721803239510.png

 

just a question, can't you find the older apps version in the collab room?

@MauroRiboniMX ,

I'm finding a limited number of images and app versions on both the US and DE collaboration rooms. Usually only 1 patch per major release.

@Bobby 

next release will be 1.20.9 for node-red and will solve that. by that time i suggest you to use the "workaround" or either move to 2.6.x Globally the fix for this problem is integrated in version: 1.20.9, 2.6.5, 3.2.0.

 

Regarding this, we are not allowed to ship the older versions, for security reasons. Checked now.
if there is for example a vulnerability, we have to patch it and we are not allowed to ship the vulnerable version anymore. 

This is the law. 


 

Bobby
Established Member

Hi, by doing so does it mean my Virtual Control Cannot access to the internet? because i still not able to install pallete.

Yes, 

That is the bug happening with the workaroung. When you do that settings that is no more working. with 1.20.9 will be fixed 

cal9mx2
Member

Where did you download the NodeRED version "NodeRED RED-V-120.0+3.0.2-ctrlx"

Did that fix the issue? I currently have a Virtual Core 1.20.12 (image version), that is imitating the issue of a physical core, that cannot be upgraded.

On the store only found version 3.1.

@CodeShepherd and @MauroRiboniMX I already tried with the newest versions and I can connect to the internet, but cannot download any plugins from the pallet manager in NodeRed. 

Here is my CtrlX Virtual version (2.6.8 image version) & my NodeRed Version (NodeRED 2.6.5+3.1.11-ctrlx). 

cal9mx2_0-1722912973583.png

cal9mx2_1-1722913346346.png

 

 

 

I leave here my newest post with more details if you can help me: NodeRED - Cannot install plugins via NodeRed Pallete Manager (InfluxDB plugin error) (boschrexroth.c...

Hello, 

Can you send here the proxy page configuration? 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist